# -*- coding: cp1252 -*- ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications, enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the user's requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND, AND IXIA # # DISCLAIMS ALL WARRANTIES, EXPRESS, IMPLIED, STATUTORY OR OTHERWISE, # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF, OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF, # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS, LOST BUSINESS, LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT, INCIDENTAL, PUNITIVE OR # # CONSEQUENTIAL DAMAGES, EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g., any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script, any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This sample configures 10 IPv4 sessions on each of the two ports # # - Adds a Quick Flow Group # # - Edit some settings for the Quick Flow Group like: frameSize, frameRate # # - Generate Traffic # # - Apply Traffic # # - Start Traffic # # # ################################################################################ if 'py' not in dir(): class TestFailedError(Exception): pass class Py: pass py = Py() py.ports = [('10.205.15.62', 3, 5), ('10.205.15.62', 3, 6)] py.ixTclServer = '10.205.15.224' py.ixTclPort = 8009 ################################################################################ # Import the IxNet library ################################################################################ import IxNetwork import time ixNet = IxNetwork.IxNet() ################################################################################ # Connect to IxNet client ################################################################################ ixNet.connect(py.ixTclServer, '-port', py.ixTclPort, '-version', '7.40') ################################################################################ # Cleaning up IxNetwork ################################################################################ print ("Cleaning up IxNetwork...") ixNet.execute('newConfig') ################################################################################ # Adding ports to configuration ################################################################################ print ("Adding ports to configuration") root = ixNet.getRoot() ixNet.add(root, 'vport') ixNet.add(root, 'vport') ixNet.commit() vPorts = ixNet.getList(root, 'vport') vport1 = vPorts[0] vport2 = vPorts[1] ################################################################################ # Adding IPv4 endpoints to configuration ################################################################################ print ("Add topologies") ixNet.add(root, 'topology') ixNet.add(root, 'topology') ixNet.commit() topo1 = ixNet.getList(root, 'topology')[0] topo2 = ixNet.getList(root, 'topology')[1] print ("Add ports to topologies") ixNet.setAttribute(topo1, '-vports', vport1) ixNet.setAttribute(topo2, '-vports', vport2) ixNet.commit() print ("Add device groups to topologies") ixNet.add(topo1, 'deviceGroup') ixNet.add(topo2, 'deviceGroup') ixNet.commit() dg1 = ixNet.getList(topo1, 'deviceGroup')[0] dg2 = ixNet.getList(topo2, 'deviceGroup')[0] print ("Add Ethernet stacks to device groups") ixNet.add(dg1, 'ethernet') ixNet.add(dg2, 'ethernet') ixNet.commit() mac1 = ixNet.getList(dg1, 'ethernet')[0] mac2 = ixNet.getList(dg2, 'ethernet')[0] print ("Add ipv4 stacks to Ethernets") ixNet.add(mac1, 'ipv4') ixNet.add(mac2, 'ipv4') ixNet.commit() ipv4_1 = ixNet.getList(mac1, 'ipv4')[0] ipv4_2 = ixNet.getList(mac2, 'ipv4')[0] print ("Setting multi values for ipv4 addresses") ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-address') + '/counter', '-start', '22.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-gatewayIp') + '/counter', '-start', '22.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_1, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-address') + '/counter', '-start', '22.1.1.2', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-gatewayIp') + '/counter', '-start', '22.1.1.1', '-step', '0.0.1.0') ixNet.setMultiAttribute(ixNet.getAttribute(ipv4_2, '-resolveGateway') + '/singleValue', '-value', 'true') ixNet.commit() ################################################################################ # Assign ports ################################################################################ vports = ixNet.getList(ixNet.getRoot(), 'vport') print ("Assigning ports to " + str(vports) + " ...") assignPorts = ixNet.execute('assignPorts', py.ports, [], ixNet.getList("/","vport"), True) if assignPorts != vports: raise TestFailedError("FAILED assigning ports. Got %s" %assignPorts) else: print("PASSED assigning ports. Got %s" %assignPorts) ################################################################################ # Start All Protocols ################################################################################ print ("Starting All Protocols") ixNet.execute('startAllProtocols') print ("Sleep 30sec for protocols to start") time.sleep(30) ################################################################################ # Create a Basic Quick Flow Group ################################################################################ print ("######################") print ("## Traffic Samples ##") print ("######################") print ('') def addBasicQuickFlowGroup(ixNet, srcPort, dstPort ): print ("- add quick flow group") quick_flow_group = ixNet.add('/traffic', 'trafficItem') ################################################################################ # Setting the quick flow group attributes ################################################################################ ixNet.setMultiAttribute(quick_flow_group, '-name', 'Quick Flow Groups', '-trafficItemType', 'quick', '-trafficType', 'raw') ixNet.commit() quick_flow_group = ixNet.remapIds(quick_flow_group)[0] ################################################################################ # Setting the endpoint set attributes ################################################################################ endpoint_set = ixNet.add(quick_flow_group, 'endpointSet') ixNet.setMultiAttribute(endpoint_set, '-destinations', [dstPort+'/protocols'], '-sources', [srcPort+'/protocols']) ixNet.commit() ################################################################################ # Set the frameSize, frameRate attributes for the first stream in endpoint set 1 ################################################################################ endpoint_set = ixNet.remapIds(endpoint_set)[0] highlevelstream1 = ixNet.getList(quick_flow_group, 'highLevelStream')[0] ixNet.setAttribute(highlevelstream1+'/frameSize', '-fixedSize', '120') ixNet.setAttribute(highlevelstream1+'/frameRate', '-rate', '500') ixNet.setAttribute(highlevelstream1+'/frameRate', '-type', 'framesPerSecond') ixNet.commit() ################################################################################ # setting the Ethernet source and destination mac addresses ################################################################################ for stack in ixNet.getList(highlevelstream1, 'stack'): if "ethernet-" in stack: for field in ixNet.getList(stack, 'field'): if "ethernet.header.destinationAddress-" in field: ixNet.setAttribute(field, '-singleValue', '33:00:00:00:00:00') elif "ethernet.header.sourceAddress-" in field: ixNet.setAttribute(field, '-singleValue', '11:00:00:00:00:00') ixNet.commit() ################################################################################ # Add the Quick Flow Group, Generate, Apply and Start the traffic ################################################################################ print ("- Add Quick Flow Group") addBasicQuickFlowGroup(ixNet, vport1, vport2) print ("- Generate Traffic") ti1 = ixNet.getList('/traffic', 'trafficItem') ixNet.execute('generate', ti1) print ("- Apply Traffic") ixNet.execute('apply', '/traffic') print ("- Start Traffic") ixNet.execute('start', '/traffic') print ("Sleep 30sec then stop traffic") time.sleep(30) print ("- Stop Traffic") ixNet.execute('stop', '/traffic') ################################################################################ # Stop All Protocols ################################################################################ print ("Stop All Protocols") ixNet.execute('stopAllProtocols') print ("Sleep 30sec for protocols to stop") time.sleep(30)