#!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Keysight and have# # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Keysight and/or by the user and/or by a third party)] shall at all # # times remain the property of Keysight. # # # # Keysight does not warrant (i) that the functions contained in the script # # will meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND Keysight # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL KEYSIGHT BE LIABLE FOR ANY DAMAGES RESULTING FROM OR # # ARISING OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART # # THEREOF INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF Keysight HAS BEEN ADVISED OF THE POSSIBILITY OF# # SUCH DAMAGES IN ADVANCE. # # Keysight will not be required to provide any software maintenance or support# # s.ervices of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Keysight may# # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Keysight to # # provide any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF CUSP APIs. # # # # 1. It will create 2 topologies. CUSP CP with PPPoX Server is configured # # in one topology & CUSP UP with PPPoX Subscribers are configured in # # another topology. # # 2. Start all protocol. # # 3. Retrieve protocol statistics. # # 4. Retrieve protocol learned info. # # 5. OTF change PPP Subscriber Profile attribute # # 6. Stop all protocols. # ################################################################################ # Script Starts puts "!!! Test Script Starts !!!" # Edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.39.43.12 set ixTclPort 8114 set ports {{10.39.50.200 1 1} { 10.39.50.200 1 2}} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 9.20 \ -setAttribute strict puts "Creating a new config" ixNet exec newConfig # ############################################################################### # 1. Configure CUSP CP & UP # ############################################################################### puts "Adding 2 vports" ixNet add [ixNet getRoot] vport ixNet add [ixNet getRoot] vport ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vportTx [lindex $vPorts 0] set vportRx [lindex $vPorts 1] puts "Assigning the ports" ::ixTclNet::AssignPorts $ixia::ports {} $vPorts force puts "Adding 2 topologies" ixNet add [ixNet getRoot] topology -vports $vportTx ixNet add [ixNet getRoot] topology -vports $vportRx ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topo1 [lindex $topologies 0] set topo2 [lindex $topologies 1] puts "Adding 2 device groups" ixNet add $topo1 deviceGroup ixNet add $topo2 deviceGroup ixNet commit set t1devices [ixNet getList $topo1 deviceGroup] set t2devices [ixNet getList $topo2 deviceGroup] set t1dev1 [lindex $t1devices 0] set t2dev1 [lindex $t2devices 0] puts "Configuring the multipliers (number of sessions)" ixNet setAttr $t1dev1 -multiplier 1 ixNet setAttr $t2dev1 -multiplier 1 ixNet commit puts "Adding ethernet/mac endpoints" ixNet add $t1dev1 ethernet ixNet add $t2dev1 ethernet ixNet commit set mac1 [ixNet getList $t1dev1 ethernet] set mac2 [ixNet getList $t2dev1 ethernet] puts "Configuring the mac addresses" ixNet setMultiAttr [ixNet getAttr $mac1 -mac]/counter\ -direction increment \ -start {18:03:73:C7:6C:B1} \ -step {00:00:00:00:00:01} ixNet setAttr [ixNet getAttr $mac2 -mac]/singleValue\ -value {18:03:73:C7:6C:01} ixNet commit puts "Add ipv4" ixNet add $mac1 ipv4 ixNet add $mac2 ipv4 ixNet commit set ip1 [ixNet getList $mac1 ipv4] set ip2 [ixNet getList $mac2 ipv4] set mvAdd1 [ixNet getAttr $ip1 -address] set mvAdd2 [ixNet getAttr $ip2 -address] set mvGw1 [ixNet getAttr $ip1 -gatewayIp] set mvGw2 [ixNet getAttr $ip2 -gatewayIp] puts "configuring ipv4 addresses" ixNet setAttr $mvAdd1/singleValue -value "20.20.20.2" ixNet setAttr $mvAdd2/singleValue -value "20.20.20.1" ixNet setAttr $mvGw1/singleValue -value "20.20.20.1" ixNet setAttr $mvGw2/singleValue -value "20.20.20.2" ixNet setAttr [ixNet getAttr $ip1 -prefix]/singleValue -value 24 ixNet setAttr [ixNet getAttr $ip2 -prefix]/singleValue -value 24 ixNet setMultiAttr [ixNet getAttr $ip1 -resolveGateway]/singleValue -value true ixNet setMultiAttr [ixNet getAttr $ip2 -resolveGateway]/singleValue -value true ixNet commit # Add CUSP CP and CUSP UP puts "Adding CUSP CP over IP4 stacks" ixNet add $ip1 cuspCP ixNet add $ip2 cuspUP ixNet commit set cp [ixNet getList $ip1 cuspCP] set up [ixNet getList $ip2 cuspUP] # Add VXLAN GPE puts "Adding VXLAN GPE over IP4 stacks" ixNet add $ip1 vxlangpe ixNet add $ip2 vxlangpe ixNet commit set vxlangpe2 [ixNet getList $ip2 vxlangpe] # Add UP Group Info on CUSP CP ixNet add $cp upGroupInfo ixNet commit set upGroupInfo [ixNet getList $cp upGroupInfo] # Rename topologies and devices puts "Renaming the topologies and the device groups" ixNet setAttr $topo1 -name "CP with PPPoE Server" ixNet setAttr $topo2 -name "UP with PPPoE Subscribers" ixNet setAttr $t1dev1 -name "CUSP CP" ixNet setAttr $t2dev1 -name "CUSP UP" ixNet commit # Configure UP Group Info puts "Configuring UP Group Info" ixNet setAttr [ixNet getAttr $upGroupInfo -iPv4Address]/singleValue -value 20.20.20.1 ixNet setAttr [ixNet getAttr $upGroupInfo -vxlanIPv4Address]/singleValue -value 20.20.20.1 ixNet setAttr [ixNet getAttr $upGroupInfo -cpVxlanIPv4Address]/singleValue -value 20.20.20.2 ixNet setAttr $upGroupInfo -numberOfPppoeUsers 1 ixNet commit # Configure UP and VxLAN GPE ixNet setAttr [ixNet getAttr $up -cpIpv4Address]/singleValue -value 20.20.20.2 ixNet setAttr [ixNet getAttr $vxlangpe2 -vni]/singleValue -value 1000 ixNet setAttr [ixNet getAttr $vxlangpe2 -ipv4_multicast]/singleValue -value 225.0.1.1 ixNet commit # Add PPPoX Server behind CP puts "Adding PPPoX Server behind CP" ixNet add $t1dev1 deviceGroup ixNet commit set t1dev2 [lindex [ixNet getList $t1dev1 deviceGroup] 0] ixNet add $t1dev2 ethernet ixNet commit set mac11 [ixNet getList $t1dev2 ethernet] set pppServer [ixNet add $mac11 pppoxserver] ixNet commit # Add PPPoX Client beind UP puts "Adding PPPoX Client behind UP" ixNet add $t2dev1 deviceGroup ixNet commit set t2dev2 [lindex [ixNet getList $t2dev1 deviceGroup] 0] ixNet add $t2dev2 ethernet ixNet commit set mac22 [ixNet getList $t2dev2 ethernet] set pppClient [ixNet add $mac22 pppoxclient] ixNet commit ixNet setAttr $t1dev2 -multiplier 1 ixNet setAttr $t2dev2 -multiplier 1 ixNet commit # ############################################################################### # 2. Start protocols # ############################################################################### puts "Starting protocols and waiting for 45 seconds for protocols to come up" ixNet exec start $t1dev1 after 10000 ixNet exec start $t2dev1 after 10000 ixNet exec start $t1dev2 after 10000 ixNet exec start $t2dev2 after 15000 # ############################################################################### # 3. Retrieve protocol statistics. # ############################################################################### puts "Fetching CUSP CP Per Port Stats\n" set viewPage {::ixNet::OBJ-/statistics/view:"CUSP CP Per Port"/page} set statcap [ixNet getAttr $viewPage -columnCaptions] foreach statValList [ixNet getAttr $viewPage -rowValues] { foreach statVal $statValList { puts "***************************************************" set index 0 foreach satIndv $statVal { puts [format "%*s:%*s" -30 [lindex $statcap $index] -10 $satIndv] incr index } } } puts "***************************************************" # ############################################################################## # 4. Retrieve protocol learned info # ############################################################################## puts "Fetching PPP Subscriber Learned Info" ixNet exec getPppSubscriberInfo $upGroupInfo 1 after 5000 set learnedInfoList [ixNet getList $upGroupInfo learnedInfo] set linfoList [ixNet getList $learnedInfoList table] puts "PPP Subscriber learned info" puts "***************************************************" foreach table $linfoList { puts "***************************************************" set column [ixNet getAttr $table -columns] puts "$column" set values [ixNet getAttr $table -values] puts "$values\n" puts "***************************************************" } puts "***************************************************" # ############################################################################### # 5. Change PPP Subscriber Profile attributes on the fly # ############################################################################### puts "Changing PPP Subscriber Profile attributes on the fly ..." set pppoEUsersList $upGroupInfo/pppoEUsersList ixNet setAttr [ixNet getAttr $pppoEUsersList -cost]/singleValue -value 55 ixNet commit ixNet exec applyOnTheFly [ixNet getRoot]/globals/topology # ############################################################################### # 6. Stop all protocols # ############################################################################### ixNet exec stopAllProtocols puts "!!! Test Script Ends !!!"