################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # The script creates and configures 2 PPP stacks. # # Set/Get multivalue parameters. # # Start/Stop protocols. # # Module: # # The sample was tested on an FlexAP10G16S module. # ################################################################################ $py_ixTclServer = "localhost"; $py_ixTclPort = 8009; #-----------------------------------------------------------------------------------------------------------------------------------# #------------------------------------------------Import Lib and Other pl packages---------------------------------------------------# use IxNetwork; #use Time::Seconds; #use strict; #-----------------------------------------------------------------------------------------------------------------------------------# print "\n Create an instance of the IxNetwork class."; $ixNet = new IxNetwork(); print "\n Connecting to the Client.\n"; $ixNet->connect($py_ixTclServer, '-port', $py_ixTclPort, '-version', '7.30'); print "\n Clear the configuration."; $asyncHandle = $ixNet->setAsync()->execute('newConfig'); $ixNet->wait($asyncHandle); print "\n\n Adding 2 virtual ports."; $root = $ixNet->getRoot(); $vport1 = $ixNet->add($root, 'vport', '-name', 'PPP1'); $vport2 = $ixNet->add($root, 'vport', '-name', 'PPP2'); $ixNet->commit(); @vPorts = $ixNet->getList($root, 'vport'); print "\n\t\tvPorts: ",@vPorts,"\n"; $vportTx = @vPorts[0]; $vportRx = @vPorts[1]; print "\n Adding 2 topologies."; $ixNet->add($root, 'topology', '-name', 'Client Topology'); $ixNet->add($root, 'topology', '-name', 'Server Topology'); $ixNet->commit(); @topologies = $ixNet->getList($root, 'topology'); print "\n\t\tTopology: ",@topologies,"\n"; $topo1 = @topologies[0]; $topo2 = @topologies[1]; print "\n Adding deviceGroups and set multipliers."; $ixNet->add($topo1, 'deviceGroup', '-name', 'Client Device Group', '-multiplier', 20); $ixNet->add($topo2, 'deviceGroup', '-name', 'Server Device Group', '-multiplier', 1); $ixNet->commit(); @t1devices = $ixNet->getList($topo1, 'deviceGroup'); @t2devices = $ixNet->getList($topo2, 'deviceGroup'); print "\n\t\tDeviceGroup: ",@t1devices," for ",$topo1,"\n"; print "\n\t\tDeviceGroup: ",@t2devices," for ",$topo2,"\n"; $t1dev1 = @t1devices[0]; $t2dev1 = @t2devices[0]; print "\n Assign vports to topologies."; $ixNet->setAttribute($topo1, '-vports', $vportTx); $ixNet->setAttribute($topo2, '-vports', $vportRx); $ixNet->commit(); print "\n Adding ethernet layer."; $ixNet->add($t1dev1, 'ethernet'); $ixNet->add($t2dev1, 'ethernet'); $ixNet->commit(); @mac1 = $ixNet->getList($t2dev1, 'ethernet'); @mac2 = $ixNet->getList($t1dev1, 'ethernet'); print "\n Adding PPP layers. "; $ixNet->add($mac1[0], 'pppoxserver'); $ixNet->add($mac2[0], 'pppoxclient'); $ixNet->commit(); @serverT = $ixNet->getList($mac1[0], 'pppoxserver'); @clientT = $ixNet->getList($mac2[0], 'pppoxclient'); $server = $serverT[0]; $client = $clientT[0]; print "\n Set the PPP Server Sessions Count to 20."; $ixNet->setAttribute($server, '-sessionsCount', 20); $ixNet->commit(); print "\n Set NCP type to dual stack."; $multivalue_ncp1 = $ixNet->getAttribute($client, '-ncpType'); $multivalue_ncp2 = $ixNet->getAttribute($server, '-ncpType'); @multivalue_ncp_sv1 = $ixNet->getList($multivalue_ncp1, 'singleValue'); @multivalue_ncp_sv2 = $ixNet->getList($multivalue_ncp2, 'singleValue'); $ixNet->setAttribute($multivalue_ncp_sv1[0], '-value', 'dual_stack'); $ixNet->setAttribute($multivalue_ncp_sv2[0], '-value', 'dual_stack'); $ixNet->commit(); $chassis1 = '10.205.15.62'; $card1 = '2'; $port1 = '15'; $card2 = '2'; $port2 = '16'; $chassis = $ixNet->add($ixNet->getRoot().'availableHardware', 'chassis', '-hostname', $chassis1); $ixNet->commit(); @chassisItems = $ixNet->remapIds($chassis); $chassis = $chassisItems[0]; print "\n\n Assign hardware ports to virtual ports."; $ixNet->setAttribute($vport1, '-connectedTo', $chassis.'/card:'.$card1.'/port:'.$port1); $ixNet->setAttribute($vport2, '-connectedTo', $chassis.'/card:'.$card2.'/port:'.$port2); $ixNet->commit(); print "\n\n Start the PPP Server."; $ixNet->execute('start', $server); sleep(10); print "\n\n Start the PPP Client."; $ixNet->execute('start', $client); sleep(10); print "\n\n PPP Client Learned Information: \n"; @addresses_v4 = $ixNet->getAttribute($client, '-discoveredIpv4Addresses'); @addresses_v6 = $ixNet->getAttribute($client, '-discoveredIpv6Addresses'); @session_ids = $ixNet->getAttribute($client, '-discoveredSessionIds'); print "\n IPv4 Addresses: \n"; print join("\n ", @addresses_v4); print "\n IPv6 Addresses: \n"; print join("\n ", @addresses_v6); print "\n Session IDs: \n"; print join("\n ", @session_ids); print "\n\n Stop the PPP Client."; $ixNet->execute('stop', $mac2[0]); sleep(10); print "\n\n Stop the PPP Server."; $ixNet->execute('stop', $mac1[0]); sleep(10); print "\n\n Clear the configuration."; $asyncHandle = $ixNet->setAsync()->execute('newConfig'); $ixNet->wait($asyncHandle); print "\n\n Disconnect from the IxNetwork Client.\n"; $ixNet->disconnect();