#!/bin/sh # the next line restarts using tclsh \ exec tclsh "$0" "$@" ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use ping functionality # # it will configure 2 topologyes with IPv4 and than it will send ping # # in between diferent ip adresses. # # Module: # # The sample was tested on 2 back-to-back XMVDC16 ports # ################################################################################ puts "Load ixNetwork Tcl API package" package require IxTclNetwork # edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.200.115.201 ;# IP Address of the IxNetwork Tcl Server set ixTclPort 8018 ;# Port number of the IxNetwork Tcl Server set ports {{10.200.113.3 2 1} {10.200.113.3 2 2}} ;# Chassis-Slot port details {{ChassisIP Slot Port}...} } puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 7.0 –setAttribute strict puts "Create a new config" ixNet exec newConfig puts "Add 2 vport" ixNet add [ixNet getRoot] vport -name testVport1 ixNet add [ixNet getRoot] vport -name testVport2 ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vport1 [lindex $vPorts 0] set vport2 [lindex $vPorts 1] puts "Add 2 Topologies" ixNet add [ixNet getRoot] topology -name testTpg1 ixNet add [ixNet getRoot] topology -name testTpg2 ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topo1 [lindex $topologies 0] set topo2 [lindex $topologies 1] puts "Add 2 device groups with multipliers (number of sessions) as 5" ixNet add $topo1 deviceGroup -name testDg1 -multiplier 5 ixNet add $topo2 deviceGroup -name testDg2 -multiplier 5 ixNet commit set dev1 [ixNet getList $topo1 deviceGroup] set dev2 [ixNet getList $topo2 deviceGroup] puts "Add MAC" ixNet add $dev1 ethernet -name testEth1 ixNet add $dev2 ethernet -name testEth2 ixNet commit set mac1 [ixNet getList $dev1 ethernet] set mac2 [ixNet getList $dev2 ethernet] puts "Add IPv4" ixNet add $mac1 ipv4 -name testIP1 ixNet add $mac2 ipv4 -name testIP2 ixNet commit set ip1 [ixNet getList $mac1 ipv4] set ip2 [ixNet getList $mac2 ipv4] set ip1Items [ixNet getList $ip1 item] set ip2Items [ixNet getList $ip2 item] puts "Add vports to topologies" set tPort1 [lindex [ixNet getList $topo1 port] 0] set tPort2 [lindex [ixNet getList $topo2 port] 0] ixNet setAttr $topo1 -vports $vport1 ixNet setAttr $topo2 -vports $vport2 ixNet commit puts "Setting multi values for ipv4 addresses" set ip1MultivalueAddr [ixNet getAttr $ip1 -address] ixNet setMultiAttr $ip1MultivalueAddr/counter \ -direction increment \ -start 22.1.1.1 \ -step 0.0.0.2 set ip2MultivalueAddr [ixNet getAttr $ip2 -address] ixNet setMultiAttr $ip2MultivalueAddr/counter \ -direction increment \ -start 22.1.1.2 \ -step 0.0.0.2 set ip1MultivalueGw [ixNet getAttr $ip1 -gatewayIp] ixNet setMultiAttr $ip1MultivalueGw/counter \ -direction increment \ -start 22.1.1.2 \ -step 0.0.0.2 set ip2MultivalueGw [ixNet getAttr $ip2 -gatewayIp] ixNet setMultiAttr $ip2MultivalueGw/counter \ -direction increment \ -start 22.1.1.1 \ -step 0.0.0.2 ixNet setAttr [ixNet getAttr $ip1 -resolveGateway]/singleValue -value true ixNet setAttr [ixNet getAttr $ip2 -resolveGateway]/singleValue -value true ixNet commit set ip1Item1_IP [ixNet getAtt [lindex $ip1Items 0] -address] set ip1Item1_GW [ixNet getAtt [lindex $ip1Items 0] -gatewayIp] set ip2Item1_IP [ixNet getAtt [lindex $ip2Items 0] -address] set ip2Item1_GW [ixNet getAtt [lindex $ip2Items 0] -gatewayIp] puts "Assigning the ports" ::ixTclNet::AssignPorts $::ixia::ports {} $vPorts force puts "Starting protocols" ixNet exec startAllProtocols after 10000 puts "Ping IP1/Item1 Gateway from IP1/Item1" puts [ixNet exec sendPing [lindex $ip1Items 0] $ip1Item1_GW] puts "Ping IP2/Item1 from IP1/Item1" puts [ixNet exec sendPing [lindex $ip1Items 0] $ip2Item1_IP] puts "Ping IP2/Item1 from all IP1 Items" puts [ixNet exec sendPing $ip1 $ip2Item1_IP] puts "Ping a non-existing Item from IP1/Item1" puts [ixNet exec sendPing [lindex $ip1Items 0] 22.1.2.3] puts "TEST END" puts "" puts "" puts "For more info please refer to the user manual or the built-in help" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4]"