#!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use next gen protocols # # It will create 2 topologyes with ethernet and vlan stacks and than it # # will create and send traffic over them # # Module: # # The sample was tested on 2 back-to-back XMVDC16 ports # ################################################################################ # edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.200.115.201 ;# IP Address of the IxNetwork Tcl Server set ixTclPort 8018 ;# Port number of the IxNetwork Tcl Server set ports {{10.200.113.3 2 1} {10.200.113.3 2 2}} ;# Chassis-Slot port details {{ChassisIP Slot Port}...} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 7.0 –setAttribute strict puts "Create a new config" ixNet exec newConfig puts "Add 2 vport" ixNet add [ixNet getRoot] vport ixNet add [ixNet getRoot] vport ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vportTx [lindex $vPorts 0] set vportRx [lindex $vPorts 1] puts "Adding 2 topologies" ixNet add [ixNet getRoot] topology -vports $vportTx ixNet add [ixNet getRoot] topology -vports $vportRx ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topo1 [lindex $topologies 0] set topo2 [lindex $topologies 1] puts "Adding 2 device groups" ixNet add $topo1 deviceGroup ixNet add $topo2 deviceGroup ixNet commit set t1devices [ixNet getList $topo1 deviceGroup] set t2devices [ixNet getList $topo2 deviceGroup] set t1dev1 [lindex $t1devices 0] set t2dev1 [lindex $t2devices 0] puts "Configuring the multipliers (number of sessions)" ixNet setAttr $t1dev1 -multiplier 5 ixNet setAttr $t2dev1 -multiplier 1 ixNet commit puts "Adding ethernet/mac endpoints" ixNet add $t1dev1 ethernet ixNet add $t2dev1 ethernet ixNet commit set mac1 [ixNet getList $t1dev1 ethernet] set mac2 [ixNet getList $t2dev1 ethernet] puts "Enabled vlan" ixNet setAttr $mac1 -vlanCount 1 ixNet setAttr $mac2 -vlanCount 1 ixNet setAttr $mac1 -useVlans true ixNet setAttr $mac2 -useVlans true ixNet commit set vlan1 [ixNet getList $mac1 vlan] set vlan2 [ixNet getList $mac2 vlan] puts "Configuring the mac addresses" ixNet setMultiAttr [ixNet getAttr $mac1 -mac]/counter \ -direction increment \ -start {18:03:73:C7:6C:B1} \ -step {00:00:00:00:00:01} ixNet setAttr [ixNet getAttr $mac2 -mac]/singleValue \ -value {18:03:73:C7:6C:01} ixNet commit puts "Configure the vlan value" ixNet setAttr [ixNet getAttr $vlan1 -vlanId]/singleValue -value 180 ixNet setAttr [ixNet getAttr $vlan2 -vlanId]/singleValue -value 180 ixNet commit puts "Renaming the topologies and the device groups" ixNet setAttr $topo1 -name "Send Topology" ixNet setAttr $topo2 -name "Receive Topology" ixNet setAttr $t1dev1 -name "Send Device" ixNet setAttr $t2dev1 -name "Receive Device" ixNet commit puts "Creating a traffic item in between the ethernet/mac endpoints" ixNet add [ixNet getRoot]/traffic trafficItem \ -name {Ethernet L2 with vlan} \ -allowSelfDestined False \ -trafficItemType l2L3 \ -mergeDestinations False \ -egressEnabled False \ -srcDestMesh oneToOne \ -enabled True \ -routeMesh oneToOne \ -transmitMode interleaved \ -biDirectional False \ -trafficType {ethernetVlan} \ -hostsPerNetwork 1 ixNet commit set trItem [ixNet getList [ixNet getRoot]/traffic trafficItem] ixNet add $trItem endpointSet \ -sources $mac1 \ -destinations $mac2 \ -name {eps1} \ -sourceFilter {} \ -destinationFilter {} ixNet commit ixNet setMultiAttrs $trItem/configElement:1/frameSize \ -type fixed \ -fixedSize 128 ixNet setMultiAttrs $trItem/configElement:1/frameRate \ -type percentLineRate \ -rate 10 \ ixNet setMultiAttrs $trItem/configElement:1/transmissionControl \ -duration 1 \ -iterationCount 1 \ -startDelayUnits bytes \ -minGapBytes 12 \ -frameCount 1 \ -type fixedIterationCount \ -interBurstGapUnits nanoseconds \ -interBurstGap 0 \ -enableInterBurstGap False \ -interStreamGap 0 \ -repeatBurst 1 \ -enableInterStreamGap False \ -startDelay 0 \ -burstPacketCount 1 ixNet commit ixNet setMultiAttrs $trItem/tracking \ -trackBy {{sourceDestValuePair0} {ethernetIiEtherType0}} ixNet commit puts "Assigning the ports" ::ixTclNet::AssignPorts $ixia::ports {} $vPorts force puts "Starting protocols" ixNet exec startAllProtocols puts "TEST END" puts " " puts " " puts "For more info please refer to the user manual or the built-in help" puts " " puts "ixNet help ::ixNet::OBJ-/topology" puts "[ixNet help ::ixNet::OBJ-/topology]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/vlan" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/vlan]"