#!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF BFDv4 API # # It will create 2 BFDv4 topologies over VXLAN, it will start the emulation # # and than it will retrieve and display few statistics # ################################################################################ # edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.216.22.27 set ixTclPort 8229 set ports {{10.216.108.99 11 3} { 10.216.108.99 11 4}} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 8.00\ –setAttribute strict puts "Creating a new config" ixNet exec newConfig ################################################################################ # protocol configuration section # ################################################################################ puts "Adding 2 vports" ixNet add [ixNet getRoot] vport ixNet add [ixNet getRoot] vport ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vportTx [lindex $vPorts 0] set vportRx [lindex $vPorts 1] puts "Assigning the ports" ::ixTclNet::AssignPorts $ixia::ports {} $vPorts force puts "Adding 2 topologies" ixNet add [ixNet getRoot] topology -vports $vportTx ixNet add [ixNet getRoot] topology -vports $vportRx ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topo1 [lindex $topologies 0] set topo2 [lindex $topologies 1] puts "Adding 2 device groups" ixNet add $topo1 deviceGroup ixNet add $topo2 deviceGroup ixNet commit set t1devices [ixNet getList $topo1 deviceGroup] set t2devices [ixNet getList $topo2 deviceGroup] set t1dev1 [lindex $t1devices 0] set t2dev1 [lindex $t2devices 0] puts "Configuring the multipliers (number of sessions)" ixNet setAttr $t1dev1 -multiplier 1 ixNet setAttr $t2dev1 -multiplier 1 ixNet commit puts "Adding ethernet/mac endpoints" ixNet add $t1dev1 ethernet ixNet add $t2dev1 ethernet ixNet commit set mac1 [ixNet getList $t1dev1 ethernet] set mac2 [ixNet getList $t2dev1 ethernet] puts "Configuring the mac addresses" ixNet setMultiAttr [ixNet getAttr $mac1 -mac]/counter\ -direction increment \ -start {18:03:73:C7:6C:B1} \ -step {00:00:00:00:00:01} ixNet setAttr [ixNet getAttr $mac2 -mac]/singleValue\ -value {18:03:73:C7:6C:01} ixNet commit puts "Add ipv4" ixNet add $mac1 ipv4 ixNet add $mac2 ipv4 ixNet commit set ip1 [ixNet getList $mac1 ipv4] set ip2 [ixNet getList $mac2 ipv4] set mvAdd1 [ixNet getAttr $ip1 -address] set mvAdd2 [ixNet getAttr $ip2 -address] set mvGw1 [ixNet getAttr $ip1 -gatewayIp] set mvGw2 [ixNet getAttr $ip2 -gatewayIp] puts "configuring ipv4 addresses" ixNet setAttr $mvAdd1/singleValue -value "20.20.20.2" ixNet setAttr $mvAdd2/singleValue -value "20.20.20.1" ixNet setAttr $mvGw1/singleValue -value "20.20.20.1" ixNet setAttr $mvGw2/singleValue -value "20.20.20.2" ixNet setAttr [ixNet getAttr $ip1 -prefix]/singleValue -value 24 ixNet setAttr [ixNet getAttr $ip2 -prefix]/singleValue -value 24 ixNet setMultiAttr [ixNet getAttr $ip1 -resolveGateway]/singleValue -value true ixNet setMultiAttr [ixNet getAttr $ip2 -resolveGateway]/singleValue -value true ixNet commit ########################################################################### #Add and Configure VXLAN Interface ########################################################################### puts "Add VXLAN Interface" ixNet add $ip1 vxlan ixNet add $ip2 vxlan ixNet commit set vxlan1 [ixNet getList $ip1 vxlan] set vxlan2 [ixNet getList $ip2 vxlan] set vni2 [ixNet getAttr $vxlan2 -vni] set ipv4multicast2 [ixNet getAttr $vxlan2 -ipv4_multicast] ixNet setAttr $vni2/singleValue -value 1000 ixNet setAttr $ipv4multicast2/singleValue -value 225.0.1.1 ixNet commit ########################################################################### #Add and Configure BFDv4 Interface ########################################################################### puts "Add BFDv4 Interface" ixNet add $vxlan1 bfdv4Interface ixNet add $vxlan2 bfdv4Interface ixNet commit set bfdv41 [ixNet getList $vxlan1 bfdv4Interface] set bfdv42 [ixNet getList $vxlan2 bfdv4Interface] set bfdv4session1 [ixNet getList $bfdv41 bfdv4Session] set bfdv4session2 [ixNet getList $bfdv42 bfdv4Session] set remoteIP1 [ixNet getAttr $bfdv4session1 -remoteIp4] set remoteIP2 [ixNet getAttr $bfdv4session2 -remoteIp4] set remoteMac1 [ixNet getAttr $bfdv4session1 -remoteMac] set remoteMac2 [ixNet getAttr $bfdv4session2 -remoteMac] ixNet setAttr $remoteIP1/singleValue -value 20.20.20.1 ixNet setAttr $remoteIP2/singleValue -value 20.20.20.2 ixNet setAttr $remoteMac1/singleValue -value 18:03:73:C7:6C:01 ixNet setAttr $remoteMac2/singleValue -value 18:03:73:C7:6C:B1 ixNet commit set txInterval1 [ixNet getAttr $bfdv41 -txInterval] set txInterval2 [ixNet getAttr $bfdv42 -txInterval] set minRxInterval1 [ixNet getAttr $bfdv41 -minRxInterval] set minRxInterval2 [ixNet getAttr $bfdv42 -minRxInterval] puts "Configuring Tx Interval and Min Rx Interval on BFD Interface" ixNet setAttr $txInterval1/singleValue -value 2000 ixNet setAttr $txInterval2/singleValue -value 2000 ixNet setAttr $minRxInterval1/singleValue -value 2000 ixNet setAttr $minRxInterval2/singleValue -value 2000 ixNet commit ############################################################################# #Starting Protocols and Dispalying Statistics ############################################################################# puts "Starting protocols and waiting for 45 seconds for protocols to come up" ixNet exec startAllProtocols after 45000 puts "Verifying all the stats\n" set viewPage {::ixNet::OBJ-/statistics/view:"Protocols Summary"/page} set statcap [ixNet getAttr $viewPage -columnCaptions] foreach statValList [ixNet getAttr $viewPage -rowValues] { foreach statVal $statValList { puts "***************************************************" set index 0 foreach satIndv $statVal { puts [format "%*s:%*s" -30 [lindex $statcap $index]\ -10 $satIndv] incr index } } } puts "***************************************************" ############################################################################ ##On The Fly Section ############################################################################ puts "Deactivating and Then Activating BFD Interfaces" set activation [ixNet getAttr $bfdv41 -active] ixNet setAttr $activation/singleValue -value false ixNet commit set topology [ixNet getRoot]/globals/topology if {[catch {ixNet exec applyOnTheFly $topology}] == 1} { puts "error in applying on the fly change" puts "$::errorInfo" } after 10000 ixNet setAttr $activation/singleValue -value true ixNet commit set topology [ixNet getRoot]/globals/topology if {[catch {ixNet exec applyOnTheFly $topology}] == 1} { puts "error in applying on the fly change" puts "$::errorInfo" } after 10000 ############################################################################ #Fetching and Displaying Learned Information on BFDv4 Interface ############################################################################ ixNet exec getLearnedInfo $bfdv41 1 after 5000 set linfo [ixNet getList $bfdv41 learnedInfo] set values [ixNet getAttribute $linfo -values] puts "BFD learned info" puts "***************************************************" foreach v $values { puts $v } puts "***************************************************" puts " " puts "For more info please refer to the user manual or the built-in help" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4/bfdv4Interface" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4/bfdv4Interface]" puts "Stopping all protocols" ixNet exec stopAllProtocols puts "*********************************************************************END*************************************************************************"