#!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use BGP Large Community # # (RFC8092). # # It will create 2 BGP topologies, add IPv4 prefix pools to them, enable # # Large Community in one of them,modify the Number of Large Communities, # # and will start the emulation .It will then retrieve and display Learned # # info statistics. # ################################################################################ # edit this variables values to match your setup namespace eval ::ixia { set ixTclServer 10.39.50.121 set ixTclPort 8019 set ports {{10.39.50.123 9 7} { 10.39.50.123 9 8}} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 8.50\ –setAttribute strict puts "Creating a new config" ixNet exec newConfig ################################################################################ # protocol configuration section # ################################################################################ puts "Adding 2 vports" ixNet add [ixNet getRoot] vport ixNet add [ixNet getRoot] vport ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vportTx [lindex $vPorts 0] set vportRx [lindex $vPorts 1] puts "Assigning the ports" ::ixTclNet::AssignPorts $ixia::ports {} $vPorts force puts "Adding 2 topologies" ixNet add [ixNet getRoot] topology -vports $vportTx ixNet add [ixNet getRoot] topology -vports $vportRx ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topology1 [lindex $topologies 0] set topology2 [lindex $topologies 1] puts "Adding 2 device groups" ixNet add $topology1 deviceGroup ixNet add $topology2 deviceGroup ixNet commit set deviceGroup_T1 [ixNet getList $topology1 deviceGroup] set deviceGroup_T2 [ixNet getList $topology2 deviceGroup] set deviceGroup_T1 [lindex $deviceGroup_T1 0] set deviceGroup_T2 [lindex $deviceGroup_T2 0] puts "Configuring the multipliers (number of sessions)" ixNet setAttr $deviceGroup_T1 -multiplier 1 ixNet setAttr $deviceGroup_T2 -multiplier 1 ixNet commit puts "Adding ethernet/mac endpoints" ixNet add $deviceGroup_T1 ethernet ixNet add $deviceGroup_T2 ethernet ixNet commit set mac1 [ixNet getList $deviceGroup_T1 ethernet] set mac2 [ixNet getList $deviceGroup_T2 ethernet] puts "Configuring the mac addresses" ixNet setMultiAttr [ixNet getAttr $mac1 -mac]/counter\ -direction increment \ -start {18:03:73:C7:6C:B1} \ -step {00:00:00:00:00:01} ixNet setAttr [ixNet getAttr $mac2 -mac]/singleValue\ -value {18:03:73:C7:6C:01} ixNet commit puts "Add ipv4" ixNet add $mac1 ipv4 ixNet add $mac2 ipv4 ixNet commit set ip1 [ixNet getList $mac1 ipv4] set ip2 [ixNet getList $mac2 ipv4] set mvAdd1 [ixNet getAttr $ip1 -address] set mvAdd2 [ixNet getAttr $ip2 -address] set mvGw1 [ixNet getAttr $ip1 -gatewayIp] set mvGw2 [ixNet getAttr $ip2 -gatewayIp] puts "configuring ipv4 addresses" ixNet setAttr $mvAdd1/singleValue -value "20.20.20.2" ixNet setAttr $mvAdd2/singleValue -value "20.20.20.1" ixNet setAttr $mvGw1/singleValue -value "20.20.20.1" ixNet setAttr $mvGw2/singleValue -value "20.20.20.2" ixNet setAttr [ixNet getAttr $ip1 -prefix]/singleValue -value 24 ixNet setAttr [ixNet getAttr $ip2 -prefix]/singleValue -value 24 ixNet setMultiAttr [ixNet getAttr $ip1 -resolveGateway]/singleValue -value true ixNet setMultiAttr [ixNet getAttr $ip2 -resolveGateway]/singleValue -value true ixNet commit puts "Adding BGP over IP4 stack" ixNet add $ip1 bgpIpv4Peer ixNet add $ip2 bgpIpv4Peer ixNet commit set bgp1 [ixNet getList $ip1 bgpIpv4Peer] set bgp2 [ixNet getList $ip2 bgpIpv4Peer] puts "Enabling BGP IPv4 unicast Capability" set cap1 [ixNet getAttr $bgp1 -capabilityIpV4Unicast] set cap2 [ixNet getAttr $bgp2 -capabilityIpV4Unicast] set sv1 [ixNet getList $cap1 singleValue] set sv2 [ixNet getList $cap2 singleValue] ixNet setAttr $sv1 -value true ixNet setAttr $sv2 -value true ixNet commit puts "Enabling BGP Filter IPv4 Unicast" set filter1 [ixNet getAttr $bgp1 -filterIpV4Unicast] set filter2 [ixNet getAttr $bgp2 -filterIpV4Unicast] set sv1 [ixNet getList $filter1 singleValue] set sv2 [ixNet getList $filter2 singleValue] ixNet setAttr $sv1 -value true ixNet setAttr $sv2 -value true ixNet commit puts "Renaming the topologies and the device groups" ixNet setAttr $topology1 -name "BGP Topology 1" ixNet setAttr $topology2 -name "BGP Topology 2" ixNet setAttr $deviceGroup_T1 -name "BGP Topology 1 Router" ixNet setAttr $deviceGroup_T2 -name "BGP Topology 2 Router" ixNet commit puts "Setting IPs in BGP DUT IP tab" ixNet setAttr [ixNet getAttr $bgp1 -dutIp]/singleValue -value "20.20.20.1" ixNet setAttr [ixNet getAttr $bgp2 -dutIp]/singleValue -value "20.20.20.2" ixNet commit puts "Adding the NetworkGroup with Routers at back of it" ixNet exec createDefaultStack $deviceGroup_T1 ipv4PrefixPools ixNet exec createDefaultStack $deviceGroup_T2 ipv4PrefixPools set networkGroup_T1 [lindex [ixNet getList $deviceGroup_T1 networkGroup] 0] set networkGroup_T2 [lindex [ixNet getList $deviceGroup_T2 networkGroup] 0] ixNet setAttr $networkGroup_T1 -name "BGP_1_Network_Group1" ixNet setAttr $networkGroup_T2 -name "BGP_2_Network_Group1" ixNet commit set IPv4Pool_T1 [ixNet getList $networkGroup_T1 ipv4PrefixPools] ixNet commit after 5000 ; #Wait for the commit to take place. set IPv4Pool_T2 [ixNet getList $networkGroup_T2 ipv4PrefixPools] ixNet commit after 5000;# Wait for the commit to take place. #Persuing IPv4 Prefix Pool below #+++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ set bgpV4IPRoutePropertyPri_T1 [ixNet getList $IPv4Pool_T1 bgpIPRouteProperty] set LargeComm_v4_T1 $bgpV4IPRoutePropertyPri_T1/bgpNonVPNRRLargeCommunitiesList set EnableLargeComm_v4_T1 [ixNet getAttribute $bgpV4IPRoutePropertyPri_T1 -enableLargeCommunities] set singleValue_v4_T1 [ixNet getList $EnableLargeComm_v4_T1 singleValue] ixNet setAttribute $singleValue_v4_T1 -value true ixNet commit after 5000;# Wait for the commit to take place. #puts "Modifying the Number of LargeCommunities\n" ixNet setAttrib $bgpV4IPRoutePropertyPri_T1 -noOfLargeCommunities 3 ixNet commit after 5000;# Wait for the commit to take place. set LargeComm1_v4pool_T1 [lindex [ixNet getList $bgpV4IPRoutePropertyPri_T1 bgpNonVPNRRLargeCommunitiesList] 0] set LargeComm2_v4pool_T1 [lindex [ixNet getList $bgpV4IPRoutePropertyPri_T1 bgpNonVPNRRLargeCommunitiesList] 1] set LargeComm3_v4pool_T1 [lindex [ixNet getList $bgpV4IPRoutePropertyPri_T1 bgpNonVPNRRLargeCommunitiesList] 2] set LargeComm2_v4Pool_T1_attr [ixNet getAttribute $LargeComm2_v4pool_T1 -largeCommunity] ixNet commit after 5000;# Wait for the commit to take place. set LargeComm2_v4Pool_T1_attr_str [ixNet add $LargeComm2_v4Pool_T1_attr "string"] ixNet setAttribute $LargeComm2_v4Pool_T1_attr_str -pattern "\{Inc:\ 85550,10\}:\{Dec:\ 100,10\}:70" ixNet commit after 5000;# Wait for the commit to take place. # --------------------------------------------------------------------------- # Starting Topology # --------------------------------------------------------------------------- ################################################################################ # Start protocol and check statistics # ################################################################################ puts "Starting protocols and waiting for 45 seconds for protocols to come up" ixNet exec startAllProtocols after 45000 puts "Verifying all the stats\n" set viewPage {::ixNet::OBJ-/statistics/view:"Protocols Summary"/page} set statcap [ixNet getAttr $viewPage -columnCaptions] foreach statValList [ixNet getAttr $viewPage -rowValues] { foreach statVal $statValList { puts "***************************************************" set index 0 foreach satIndv $statVal { puts [format "%*s:%*s" -30 [lindex $statcap $index]\ -10 $satIndv] incr index } } } puts "***************************************************" ############################################################################### # print learned info # ############################################################################### ixNet exec getIPv4LearnedInfo $bgp2 1 after 5000 set linfo [ixNet getList $bgp2 learnedInfo] set values [ixNet getAttribute $linfo -values] puts "BGP learned info" puts "***************************************************" foreach v $values { puts $v } puts "***************************************************" puts "Stopping all protocols" ixNet exec stopAllProtocols puts "*********************************************************************END*************************************************************************"