#!/usr/bin/tclsh ################################################################################ # # # Copyright 1997 - 2020 by IXIA Keysight # # All Rights Reserved. # # # ################################################################################ ################################################################################ # # # LEGAL NOTICE: # # ============== # # The following code and documentation (hereinafter "the script") is an # # example script for demonstration purposes only. # # The script is not a standard commercial product offered by Ixia and have # # been developed and is being provided for use only as indicated herein. The # # script [and all modifications enhancements and updates thereto (whether # # made by Ixia and/or by the user and/or by a third party)] shall at all times # # remain the property of Ixia. # # # # Ixia does not warrant (i) that the functions contained in the script will # # meet the users requirements or (ii) that the script will be without # # omissions or error-free. # # THE SCRIPT IS PROVIDED "AS IS" WITHOUT WARRANTY OF ANY KIND AND IXIA # # DISCLAIMS ALL WARRANTIES EXPRESS IMPLIED STATUTORY OR OTHERWISE # # INCLUDING BUT NOT LIMITED TO ANY WARRANTY OF MERCHANTABILITY AND FITNESS FOR # # A PARTICULAR PURPOSE OR OF NON-INFRINGEMENT. # # THE ENTIRE RISK AS TO THE QUALITY AND PERFORMANCE OF THE SCRIPT IS WITH THE # # USER. # # IN NO EVENT SHALL IXIA BE LIABLE FOR ANY DAMAGES RESULTING FROM OR ARISING # # OUT OF THE USE OF OR THE INABILITY TO USE THE SCRIPT OR ANY PART THEREOF # # INCLUDING BUT NOT LIMITED TO ANY LOST PROFITS LOST BUSINESS LOST OR # # DAMAGED DATA OR SOFTWARE OR ANY INDIRECT INCIDENTAL PUNITIVE OR # # CONSEQUENTIAL DAMAGES EVEN IF IXIA HAS BEEN ADVISED OF THE POSSIBILITY OF # # SUCH DAMAGES IN ADVANCE. # # Ixia will not be required to provide any software maintenance or support # # services of any kind (e.g. any error corrections) in connection with the # # script or any part thereof. The user acknowledges that although Ixia may # # from time to time and in its sole discretion provide maintenance or support # # services for the script any such services are subject to the warranty and # # damages limitations set forth herein and will not obligate Ixia to provide # # any additional maintenance or support services. # # # ################################################################################ ################################################################################ # # # Description: # # This script intends to demonstrate how to use NGPF OF Controller API # # It will create one OF Controller topology , it will start the emulation # # and then it will retrieve and display few statistics . # # It will send learned info trigger for specified match crteria # ################################################################################ ################################################################################ #Procedure for Adding Match Criteria & Instruction Action Example : adding match# #criteria as IPv4, Ethernet # ################################################################################ proc enableMatchesInstructions { flowProfile requiredMatchCriteriaList requiredInstruction requiredAction } { set preDefinedTemplate [ixNet add ::ixNet::OBJ-/globals/topology/openFlowController/flowSetTemplate predefined ] set flowTemplates [ixNet add $preDefinedTemplate flowTemplate] ixNet commit after 2000 set matchActionList [ixNet getList $flowTemplates matchAction] puts "matchActionList= $matchActionList " foreach matchAction $matchActionList { if { [regexp {Blank Template} [ixNet getA $matchAction -name] ] } { ixNet exec addFromTemplate $flowProfile $matchAction ixNet commit after 2000 break } } set flowProfileMatchAction [ixNet getList $flowProfile matchAction] puts " flowProfileMatchAction = $flowProfileMatchAction " set flowProfilematchCriteria [ixNet getList $flowProfileMatchAction matchCriteria] puts " flowProfilematchCriteria = $flowProfilematchCriteria " set matchCriteriaList [ixNet getList $flowProfilematchCriteria matchCriteria] puts " matchCriteriaList = $matchCriteriaList " foreach requiredMatchCriteria $requiredMatchCriteriaList { foreach matchCriteria $matchCriteriaList { if { [string match $requiredMatchCriteria [ixNet getA $matchCriteria -name] ] } { ixNet setA $matchCriteria -isEnabled true ixNet commit after 2000 if { [string match "Ethernet" [ixNet getA $matchCriteria -name] ] } { puts "Enabling Ethernet match Criteria !!!" set ethernetmatchCriteria [ixNet getList $matchCriteria matchCriteria] foreach ethernetValue $ethernetmatchCriteria { if {[string match "Ethernet Source" [ixNet getA $ethernetValue -name] ]} { ixNet setAttr $ethernetValue -isEnabled true ixNet commit set EthernetFields [ixNet getList $ethernetValue field] set value [lindex $EthernetFields 0] set valueMulti [ixNet getAttr $value -value] set EthernetCounterVal [ixNet add $valueMulti "singleValue"] ixNet setMultiAttribute $EthernetCounterVal -value "11:0:0:0:0:0" ixNet commit set mask [lindex $EthernetFields 1] set maskMulti [ixNet getAttr $mask -value] set EthernetMaskVal [ixNet add $maskMulti "singleValue"] ixNet setMultiAttribute $EthernetMaskVal -value "ff:ff:ff:ff:ff:fe" ixNet commit } else { ixNet setAttr $ethernetValue -isEnabled true ixNet commit set EthernetDestFields [ixNet getList $ethernetValue field] set value [lindex $EthernetDestFields 0] set valueMulti [ixNet getAttr $value -value] set EthernetCounterVal [ixNet add $valueMulti "singleValue"] ixNet setMultiAttribute $EthernetCounterVal -value "12:0:0:0:0:0" ixNet commit set mask [lindex $EthernetDestFields 1] set maskMulti [ixNet getAttr $mask -value] set EthernetMaskVal [ixNet add $maskMulti "singleValue"] ixNet setMultiAttribute $EthernetMaskVal -value "ff:ff:ff:ff:ff:ff" ixNet commit } } } if { [string match $requiredMatchCriteria [ixNet getA $matchCriteria -name] ] } { ixNet setA $matchCriteria -isEnabled true ixNet commit after 2000 if { [string match "IP" [ixNet getA $matchCriteria -name] ] } { puts "Enabling IP match Criteria !!!" set IPmatchCriteria [ixNet getList $matchCriteria matchCriteria] set Ipv4matchCriteria [lindex $IPmatchCriteria 0] set IPv4List [ixNet getL $Ipv4matchCriteria matchCriteria] foreach Ipv4Value $IPv4List { if {[string match "IPv4 Source" [ixNet getA $Ipv4Value -name] ]} { ixNet setAttr $Ipv4Value -isEnabled true ixNet commit set IPv4Fields [ixNet getList $Ipv4Value field] set value [lindex $IPv4Fields 0] set valueMulti [ixNet getAttr $value -value] set IPCounterVal [ixNet add $valueMulti "singleValue"] ixNet setMultiAttribute $IPCounterVal -value "4.4.4.4" ixNet commit set mask [lindex $IPv4Fields 1] set maskMulti [ixNet getAttr $mask -value] set IPMaskVal [ixNet add $maskMulti "singleValue"] ixNet setMultiAttribute $IPMaskVal -value "255.255.255.255" ixNet commit } else { ixNet setAttr $Ipv4Value -isEnabled true ixNet commit set IPv4DestFields [ixNet getList $Ipv4Value field] set value [lindex $IPv4DestFields 0] set valueMulti [ixNet getAttr $value -value] set Ipv4CounterVal [ixNet add $valueMulti "singleValue"] ixNet setMultiAttribute $Ipv4CounterVal -value "7.7.7.7" ixNet commit set mask [lindex $IPv4DestFields 1] set maskMulti [ixNet getAttr $mask -value] set IPv4MaskVal [ixNet add $maskMulti "singleValue"] ixNet setMultiAttribute $IPv4MaskVal -value "255.255.255.255" ixNet commit } } } set fieldList [ixNet getList $matchCriteria field] foreach field $fieldList { if { [string match "Ethernet Type" [ixNet getA $field -name] ] } { puts "Enabling Eternet Type match Criteria !!!" ixNet setA $field -isEnabled true ixNet commit set EtherTypeMultiVal [ixNet getAttr $field -value] ixNet setAttr $EtherTypeMultiVal/singleValue -value 88E7 ixNet commit } } break } } } } set flowProfileMatchAction [ixNet getList $flowProfile matchAction] set flowProfileInstruction [ixNet getList $flowProfileMatchAction instructions] puts " Adding instruction" ixNet exec addInstruction $flowProfileInstruction $requiredInstruction ixNet commit after 3000 set flowProfileInstructionAdded [ixNet getList $flowProfileInstruction instruction] puts $flowProfileInstructionAdded puts "adding 2 Action" puts $requiredAction foreach action $requiredAction { ixNet exec addAction $flowProfileInstructionAdded $action ixNet commit after 2000 } after 5000 # adding value in actions set actionsAdded [ixNet getList $flowProfileInstructionAdded actions] set actions [lindex $actionsAdded 0] set actionList [ixNet getList $actions action] puts $actionList foreach action $actionList { if {[string match "Set Ethernet Source" [ixNet getA $action -name] ]} { puts "action is Set Ethernet Source" set val "4:6:0:0:0:0" } else { puts "action is Set Ethernet Destination" set val "7:7:4:8:1:7" } set field [ixNet getList $action field ] set actionValue [ixNet getAttr $field -value] ixNet setAttr $actionValue/singleValue -value $val ixNet commit after 2000 } } ################################################################################ #edit this variables values to match your setup# ################################################################################ namespace eval ::ixia { set ixTclServer 10.214.101.141 set ixTclPort 8009 set ports {{12.0.1.253 5 9} { 12.0.1.253 5 10}} } puts "Load ixNetwork Tcl API package" package req IxTclNetwork puts "Connect to IxNetwork Tcl server" ixNet connect $::ixia::ixTclServer -port $::ixia::ixTclPort -version 8.10\ –setAttribute strict puts "Creating a new config" ixNet exec newConfig ################################################################################ # protocol configuration section # ################################################################################ puts "Adding 1 vports" ixNet add [ixNet getRoot] vport ixNet commit set vPorts [ixNet getList [ixNet getRoot] vport] set vportTx [lindex $vPorts 0] puts "Assigning the ports" ::ixTclNet::AssignPorts $ixia::ports {} $vPorts force puts "Adding topology" ixNet add [ixNet getRoot] topology -vports $vportTx ixNet commit set topologies [ixNet getList [ixNet getRoot] topology] set topo1 [lindex $topologies 0] puts "Adding a device group" ixNet add $topo1 deviceGroup ixNet commit set t1devices [ixNet getList $topo1 deviceGroup] set t1dev1 [lindex $t1devices 0] puts "Configuring the multipliers (number of sessions)" ixNet setAttr $t1dev1 -multiplier 1 ixNet commit puts "Adding ethernet" set ethernet [ixNet add $t1dev1 ethernet] ixNet commit puts "Add ipv4" ixNet add $ethernet ipv4 ixNet commit set ip1 [ixNet getList $ethernet ipv4] set mvAdd1 [ixNet getAttr $ip1 -address] set mvGw1 [ixNet getAttr $ip1 -gatewayIp] puts "configuring ipv4 addresses" ixNet setAttr $mvAdd1/singleValue -value "1.1.1.2" ixNet setAttr $mvGw1/singleValue -value "1.1.1.1" ixNet setAttr [ixNet getAttr $ip1 -prefix]/singleValue -value 24 ixNet setMultiAttr [ixNet getAttr $ip1 -resolveGateway]/singleValue -value true ixNet commit puts "Renaming the topologies and the device groups" ixNet setAttr $topo1 -name "OF Controller" ixNet commit set OFController [ixNet add $ip1 openFlowController] ixNet commit set topology [lindex [ixNet getList $root topology] 0] set deviceGroup [lindex [ixNet getList $topology deviceGroup] 0] set ethernet [lindex [ixNet getList $deviceGroup ethernet] 0] set ipv4 [lindex [ixNet getList $ethernet ipv4] 0] set openFlowController1 [lindex [ixNet getList $ipv4 openFlowController] 0] puts "Set Number of OF Controller Channel to 1" set NumChannels [ixNet getAttribute $openFlowController1 -numberOfChannels] ixNet setAttr $openFlowController1 -numberOfChannels 1 ixNet commit set openFlowChannel [ixNet getL $openFlowController1 openFlowChannel] puts "Set Number of Group Per Channel to 1" set groupNum [ixNet getAttribute $openFlowChannel -groupsPerChannel] ixNet setMultiAttribute $openFlowChannel -groupsPerChannel 1 ixNet commit puts "Set Number of Meters Per Channel to 1" set meterNum [ixNet getAttribute $openFlowChannel -metersPerChannel] ixNet setMultiAttribute $openFlowChannel -metersPerChannel 1 ixNet commit puts "Set Number of FlowSet Per Channel to 1" set table [ixNet getL $openFlowChannel tables] ixNet getAttr $table -numberOfFlowSet ixNet setMultiAttribute $table -numberOfFlowSet 1 ixNet commit puts "Set Number of Flows Per Channel to 1" set flowSet [ixNet getL $table flowSet] set numFlows [ixNet getAttr $flowSet -numberOfFlows] set numFlowsValue [ixNet setMultiAttribute $flowSet -numberOfFlows 1] ixNet commit ################################################################################ #adding match criteria and instruction actions from Proc named enableMatchesInstructions# ################################################################################ set flowProfile [ixNet getL $flowSet flowProfile] set requiredMatchCriteriaList {"Ethernet" "IP"} set requiredInstruction {"Apply Actions"} set requiredAction {"Set Ethernet Source" "Set Ethernet Destination"} enableMatchesInstructions $flowProfile $requiredMatchCriteriaList $requiredInstruction $requiredAction ################################################################################ # Start protocol and check statistics # ################################################################################ puts "Starting protocols and waiting for 45 seconds for protocols to come up" ixNet exec startAllProtocols after 60000 puts "Verifying all the stats\n" set viewPage {::ixNet::OBJ-/statistics/view:"Protocols Summary"/page} set statcap [ixNet getAttr $viewPage -columnCaptions] foreach statValList [ixNet getAttr $viewPage -rowValues] { foreach statVal $statValList { puts "***************************************************" set index 0 foreach satIndv $statVal { puts [format "%*s:%*s" -30 [lindex $statcap $index]\ -10 $satIndv] incr index } } } puts "***************************************************" puts "Verifying OpenFlow Controller per port stats\n" set viewPage {::ixNet::OBJ-/statistics/view:"OpenFlow Controller Per Port"/page} set statcap [ixNet getAttr $viewPage -columnCaptions] foreach statValList [ixNet getAttr $viewPage -rowValues] { foreach statVal $statValList { puts "***************************************************" set index 0 foreach satIndv $statVal { puts [format "%*s:%*s" -30 [lindex $statcap $index]\ -10 $satIndv] incr index } } } puts "***************************************************" ################################################################################ # On the fly section (Changing Instruction Action for Set Ethernet Source field) # ################################################################################ set flowProfileMatchAction [ixNet getList $flowProfile matchAction] set flowProfileInstruction [ixNet getList $flowProfileMatchAction instructions] set flowProfileInstructionAdded [ixNet getList $flowProfileInstruction instruction] set First_action [lindex $flowProfileInstructionAdded 0] set actionsAdded [ixNet getList $First_action actions] set actionList [ixNet getList $actionsAdded action] set setEthernetSourceaction [lindex $actionList 0] if {[string match "Set Ethernet Source" [ixNet getA $setEthernetSourceaction -name] ]} { puts "Modifying Set Ethernet Source Value OTF to 76:44:33:2:1:1" set val 76:44:33:2:1:1 } set Ethernetfield [ixNet getList $setEthernetSourceaction field ] set actionValue [ixNet getAttr $Ethernetfield -value] ixNet setAttr $actionValue/singleValue -value $val ixNet commit set globals [ixNet getRoot]/globals set topology $globals/topology ixNet exec applyOnTheFly $topology ############################################################################### # print learned info # ############################################################################### ixNet exec getOFChannelLearnedInfo $openFlowController1 1 after 5000 puts "Getting Basic Controller Learned info!!!!!!!" set learnedInfoList [ixNet getL $openFlowController1 learnedInfo] set learnedInfo [lindex $learnedInfoList end] set table [lindex [ixNet getList $learnedInfo table] 0] set learnedInfoColumnsList [ixNet getAttr $table -columns] set learnedInfoValuesList [ixNet getAttr $table -values] set row2 [lindex $learnedInfoValuesList 1] puts "***************************************************" foreach v $learnedInfoColumnsList { puts $v } puts "***************************************************" puts "***************************************************" foreach v $row2 { puts $v } puts "***************************************************" puts "Getting Detailed Controller Learned info!!!!!!!" set learnedInfoList [ixNet getL $openFlowController1 learnedInfo] set learnedInfo1 [lindex $learnedInfoList 0] set table1 [lindex [ixNet getList $learnedInfo1 table] 0] set learnedInfoColumnsList [ixNet getAttr $table1 -columns] set learnedInfoValuesList [ixNet getAttr $table1 -values] set row2 [lindex $learnedInfoValuesList 0] puts "***************************************************" foreach v $learnedInfoColumnsList { puts $v } puts "***************************************************" puts "***************************************************" foreach v $row2 { puts $v } puts "***************************************************" puts "Set on demand message for flow stat!!!!" set OfChanneLearnedinfoList [ixNet getL $openFlowController1 ofChannelLearnedInfoList] set OnDemandMessage [ixNet getAttr $OfChanneLearnedinfoList -onDemandMessages] set values1 [ixNet getAttr $OnDemandMessage -values] ixNet setAttribute $OnDemandMessage/singleValue -value flowstat puts "sending on demand message on the fly for flow stat learned info" ixNet exec sendOnDemandMessage $OfChanneLearnedinfoList 1 puts " " puts "For more info please refer to the user manual or the built-in help" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet]" puts " " puts "ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4" puts "[ixNet help ::ixNet::OBJ-/topology/deviceGroup/ethernet/ipv4]" puts " " puts "ixNet help ::ixNet::OBJ-/topology:1/deviceGroup:1/ethernet:1/ipv4:1/openFlowController:1" puts "[ixNet help ::ixNet::OBJ-/topology:1/deviceGroup:1/ethernet:1/ipv4:1/openFlowController:1]" puts " " puts "[ixNet help [ixNet getRoot]/traffic]" after 15000 puts "Stopping all protocols" ixNet exec stopAllProtocols puts "*********************************************************************END*************************************************************************"