# DESCRIPTION # # This is an ixVm chassis builder parameters file used in conjunction with ixVmChassisBuilder.py. # # NOTE # # For removing, you have TWO options. # 1> Remove 'all' # 2> Remove a list of mgmtIp. # # You MUST uncomment vmMgmtCardListToRemove if you want to remove a list. # MANDATORY PARAMETERS: apiServerIp = '192.168.70.127' apiServerIpPort = '11009' hypervisorType = 'vmware' ;# vmware or qemu vChassisIp = '192.168.70.11' username = 'admin' password = 'admin' # For ADDING cards: Set ixvmCardPortList variable with a list of mgmtIp. ixvmCardPortList = [ {'mgmtIp': '192.168.70.12', 'promiscuousMode': False, 'mtu': '1500', 'keepAlive': '300'}, {'mgmtIp': '192.168.70.13', 'promiscuousMode': False, 'mtu': '1500', 'keepAlive': '300'} ] # For REMOVING cards: # Method 1: To remove all cards by default, set vmMgmtCardListToRemove = 'all' # Method 2: To remove specific cards, state the mgmt IP addresses in a list. # Method 1 vmMgmtCardListToRemove = 'all' # Method 2 A list of all the IxVmCard mgmt IP addresses to remove. #vmMgmtCardListToRemove = ['192.168.70.12', '192.168.70.13'] # Do you want to delete the virtual chassis? True or False removeVChassis = True