""" tapsettings_ApplicationSelect.py: - Connect to the API server - In this test, do the following: - Add two real ports - Add two vports - Assign two real ports in to vports - Find the transceiverOptions from vport tapsettings - Update reqAppSel attributes of transceiverOptions Supports IxNetwork API servers: - Windows, Windows Connection Mgr and Linux Requirements: - Minimum IxNetwork 10.00 - Python 2.7 and 3+ - pip install requests - pip install ixnetwork_restpy RestPy Doc: https://openixia.github.io/ixnetwork_restpy/#/overview Usage: - Enter: python